Technical FAQs

Ask a Question

What are the benefits of a KNX system at the planning stage?

There are many benefits to the KNX system at the planning stage some key points to keep mind are as follows

Functions from different areas can be linked together.
Later changes and additions can simply be inserted and do not require the complete replanning of the installation and wiring.
Modifications and extensions are still possible after many years.
Devices from different manufacturers work together on the basis of the functionalities defined in EN50090.

Its also possible to plan a range of installations with KNX system from simple installs to complete complex building management functions.
Was this helpful?
What can we do to improve the information ?