Technical FAQs

Ask a Question

What is the part number for the remote reset for the GV7 Thermal Magnetic Circuit Breakers?

The GV7 is a TeSys product built on Compact NS base.
The remote reset control used for our GV7, is the same remote reset control units used  for the Compact NS range

Therefore: For the GV7
From GV7R*20 to GV7R*150 Amps you will have to order the reference 29441.
For GV7R*220 you will have to order the reference 31549.
To discuss the references 29441 & 31549, call the helpdesk on 0870 608 8 608 & ask for Low Voltage Distribution
 
Was this helpful?
What can we do to improve the information ?