Browse FAQs

Manual Removal of PowerChute Personal Edition on Windows Systems

Published date: 22 July 2019

Issue:
Uninstallation of PowerChute Personal Edition fails or is incomplete.

Product:
PowerChute Personal Edition (PCPE)

Environment:
Windows XP, Vista, Windows 7, Windows 8, Windows 10

Cause:
Incomplete or failed uninstallation

Solution:

NOTE: Editing the system registry improperly can cause system damage. Schneider Electric is not responsible for any consequence caused by editing of the system registry.

Please review the corresponding Microsoft Kbase concerning the system registry before proceeding https://support.microsoft.com/en-us/help/322756/how-to-back-up-and-restore-the-registry-in-windows

You will want to kill the PowerChute.exe, apcsystray.exe, mainserve.exe, and dataserv.exe processes if running before you do the following steps
 

1. From the installation directory in Explorer

(e.g. 32 Bit - C:\Program Files\APC\APC PowerChute Personal Edition

64 Bit - C:\Program Files (x86)\APC\APC PowerChute Personal Edition remove the entire contents from the first 'APC' down, that is assuming you used the default path and you do not have any other APC products installed.

 

2.a In the Registry (open by going to Start->Run->type 'regedit') a. go to the

32 bit - 'My Computer\HKEY_LOCAL_MACHINE\Software\APC' key.

64 bit - 'My Computer\HKEY_LOCAL_MACHINE\Software\Wow6432Node\APC.

If you do not have any other APC products installed delete the entire APC key, otherwise just delete the APC PowerChute Personal Edition key.
 

2.b Go to the registry

32 Bit - My Computer\HKEY_LOCAL_MACHINE\Software\Microsoft\Windows\CurrentVersion\Uninstall

64 Bit - My Computer\HKEY_LOCAL_MACHINE\Software\Wow6432Node\Microsoft\Windows\CurrentVersion\Uninstall and then search for PowerChute Personal Edition.
This should return a key with the following contents:
DisplayName
UninstallString.
Remove the entire key where the match occurs.
*Note: Keep a track on the 'name of the string', it should be something like {F1486DE6-CC2E-48C0-AD20-C2C142FA1636}, but this will be depend on what Windows installer assign to it.

64 Bit - running PowerChute Personal Edition 3.1 the uninstaller is in My Computer\HKEY_LOCAL_MACHINE\Software\Wow6432Node\Microsoft\Windows\CurrentVersion\Uninstall\APC

 

2.c Go to registry on both 32 bit and 64 bit machines - 'My Computer\HKEY_LOCAL_MACHINE\Software\Classes\Installer\Products\'

search for 'PowerChute Personal Edition'.

This should return a key with the following content:

ProductName

Remove the entire key where the match occurs

3. If there is still an issue run Microsoft Fix It

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.