Browse FAQs

How much exhaust clearance is needed for a NetShelter CX cabinet?

Published date: 05 August 2019

 

Issue:
The NetShelter CX may overheat if there is not proper clearance for airflow.
 
Product Line:
NetShelter CX
 
Environment:
All models and serial ranges.
 
 
Cause:
Improper spacing can cause overheating.
 
Resolution :
See attached file.
 
NetShelter CX Wall Clearance
 
 
The exhaust fans of the NetShelter CX vent to the sides. The back of the cabinet can be placed against a wall if desired.
If the cabinet is being installed in a corner please leave at least 6 inches of open space between the side of the NetShelter CX and the wall.
It is not recommended to install a NetShelter S X where the back and both sides are against a wall.
Please see attached file for a graphic depiction of the clearance.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.