Browse FAQs

Wireless Adapters Supported in NetBotz 420

Published date: 15 July 2019

Issue:

Wireless Adapters Supported in NetBotz 420

Product Line:

NetBotz

Environment:

NetBotz 420

Cause:

The following 802.11 PC Card slot adapters are supported in the NetBotz 420 (NBRK0420 and NBWL0420)

Resolution:


* D-Link DCF-660W
* Linksys WCF12


The following GPRS / GSM compact card adapters are supported in the NetBotz 420:

ANYCOM GS-320 GPRS CF Card
ENFORA GSM0110
PRETEC CompactGPRS
Option Globesurfer ICON USB (HSDPA/UMTS/EDGE/GPRS/GSM)
http://www.option.com/products/globesurfer_icon.shtml

MultiModem GPRS USB (non-USB interface versions not supported)
http://www.multitech.com/PRODUCTS/Families/MultiModemGPRS/

MultiModem EDGE USB (non-USB interface versions not supported)
http://www.multitech.com/PRODUCTS/Families/MultiModemEDGE/

NetBotz 420 is discontinued and no longer supported. 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.