Browse FAQs

What do I do when the included exhaust ducts for our InRow SC are too short for our needs?

Published date: 31 July 2019

Issue:
What do I do when the included exhaust ducts for our InRow SC are too short for our needs?
 
Product line:
ACSC100
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
Application Note 109 outlines various considerations for the condenser section to ensure proper operation. Application Note 109 will answer how to account for the need for the need of a longer duct run and the maximum operational length of the exhaust ducts.

Please also note condenser air drawn from parking garages, industrial zones, coastal areas, or other areas with air contaminants or air entrained with corrosive chemicals is prohibited. The InRow SC does not have coil coatings or other corrosion resistant materials in the condenser section. Operation in these environments can damage the unit and reduce its operating life. Condenser air drawn from environments classified as hazardous or explosive is also prohibited. The SC is not an explosion proof product; operation in environments classified as hazardous will result in damage to facilities, equipment and possibly personal injury or death.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.