Technical FAQs

Ask a Question

Which cables or pre-wired connectors can be used with which proximity or photo-electric sensors?

A list of the possible sensor cables is detailed in the tables below:


Replace the “‚óŹ” after the letter “L” in the reference by the required cable length in metres, typically either: 2, 5, or 10.

For more detail on the cable types please refer to the sensor catalogues
 
Note: For sensors with relay output or contacts, check that they are compatible with the nominal voltage and nominal current of the cabling accessory.
 
Was this helpful?
What can we do to improve the information ?