Browse FAQs

What is the replacement enclosure for a 2510KW2C?

Published date: 01 August 2019

Issue:
What is the replacement enclosure for a 2510KW2C?

Product Line:
2510 type K manual switches

Environment:
Products sold and used in the United States

Resolution:
There are two series of the 2510KW2C.  Series A and Series B.  Series A was obsoleted in January 2002. 

Series B consists of a redesigned enclosure (box) and cover assembly. The physical size of the new Series B is almost identical to the Series A except for the overall width of the enclosure (box) is slightly wider - wider by only .15` (5/32`). The mounting holes for the Series B device are identical to the old Series A device. 

Series B, the current offering are not interchangeable with the Series A boxes.  If you have a Series A box and need parts, order a new cover and box in Series B.

The Cover is 31057-529-57.  This includes the gasket.
The Box (back portion of enclosure) is 31056-080-50.
A replacement gasket only is 31056-081-01.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.