Browse FAQs

Is catalog number 3090SCCT022 a single CT or a set of CTs?

Published date: 29 July 2019

Issue:
Is catalog number 3090SCCT022 a single CT,  or a set of CTs?

Product Line:
Power Logic

Environment:
Products sold in the United States

Cause:
Product features

Resolution:
That catalog number comprises only a single CT. If three are needed, three should be ordered.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.