Browse FAQs

Can you get an external keypad on a NEMA 3R E-FLEX drive?

Published date: 26 July 2019

Issue:
External keypad option for E-Flex Nema 3R drive

Product Line:
Altivar E-Flex drives

Environment:
NEMA 3R only E-Flex drives

Cause:
Needs to order an NEMA 3R -E-Flex drive with a remote keypad display mounted on the door. 

Resolution:
The E-Flex drive is obsolete. External keypad was not available on the E-Flex. The replacement ATV660 drive also does not have an option for external keypad on Nema 3R as they are not UV protected.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.