Browse FAQs

What does the 5 indicate before the coil voltage code on the LC1K****5** or LP1K****5** contactors?

Published date: 29 July 2019

Issue:
Does the number 5 refer to the type of termination?

Product Line:
Tesys K Miniature IEC Contactors and Overload Relays

Environment:
n/a

Resolution:
The suffix 5 indicates solder pin terminal connections instead of the standard screw clamp.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.