Browse FAQs

What are the contact ratings of the 9007MS/ML type limit switch?

Published date: 26 July 2019

Issue:
Needs to know the contact ratings of a 9007MS/ML limitswitch.

Product Line:
9007MS, 9007ML Limit Switch

Environment:
9007MS/ML

Resolution:
These limit switches have contact ratings of 300V AC and DC, at up to 10 amperes. Contact ratings may be higher than connector ratings
when using some of the prewired connector products.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.