Browse FAQs

What relay should be used to provide two wire control for the Class 8903 Type PB lighting contactor?

Published date: 17 July 2019

Issue:
What relay should be used to provide two wire control for the Class 8903 Type PB lighting contactor?

Product Line:
NEMA Lighting Contactors

Environment:
Products sold and used in the United States

Cause:
Two wire control relay needed

Resolution:
Use any 2 pole relay with a Normally Open and Normally Closed contact, such as
CA2SK11**
8501XO11V**

Complete the part number by adding the appropriate voltage code.  i.e 8501XO11V02 for 120VAC, or CA2SK11G7 for 120VAC.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.