Browse FAQs

What is the continuous current rating on the 9007C62B2 contacts?

Published date: 26 July 2019

Issue:
Checking on the continuous current rating of the contacts of a 9007C62B2.

Product Line:
9007C Limit Switches

Environment:
9007C62B2

Resolution:
See Digest 173 page 19-2. It is rated for 10 amps continuous.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.