Men
Abrha Milaw 🇪🇹 2:07:05
Asefa Mengistu 🇪🇹 2:07:25
Paul Lonyangata 🇰🇪 2:07:29
Women
Gelete Burka 🇪🇹 2:22:47
Azmera Gebru 🇪🇹 2:22:52
Azmera Abreha 🇪🇹 2:23:35
Disabled athletes
Julien Casoli 🇫🇷 1:36:57
Heinz Frei 🇨🇭 1:45:37
Vitaliy Gritsenko 🇷🇺 1:46:35
Abrha Milaw 🇪🇹 2:07:05
Asefa Mengistu 🇪🇹 2:07:25
Paul Lonyangata 🇰🇪 2:07:29
Women
Gelete Burka 🇪🇹 2:22:47
Azmera Gebru 🇪🇹 2:22:52
Azmera Abreha 🇪🇹 2:23:35
Disabled athletes
Julien Casoli 🇫🇷 1:36:57
Heinz Frei 🇨🇭 1:45:37
Vitaliy Gritsenko 🇷🇺 1:46:35
Our new personal best: 0 carbon
For the seventh straight year Schneider Electric proudly sponsored the Marathon de Paris. When our commitment to offset the Paris Marathon’s carbon footprint kicked off in 2016, we compensated 50% of the event’s emissions. This year – just four editions later – we have achieved 100%.
Why the Livelihoods Hifadhi project matters
50,000
hectares is the area of forest Kenya loses every year
150,000
cookstoves will be sold over 2013–2022
$2
is the price of one cookstove
60%
is the reduction in wood use, compared to the traditional stove
13,000
tons is the amount of wood the project will save over 10 years
1 million
tons of CO₂ is the total offset target of the project