{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the iC60H RCBO's be used on a 110V AC System?

A 110V version of the iC60H RCBO is available which is suitable for use on a standard 0 - 110V AC TN-S earthing system

A suitable RCBO to use would be the A9D198** range - ** = Amperage of the RCBO

If the 110V AC supply is 55 -0- 55V AC, the iC60H2 RCBO must be used

A suitable RCBO to use would be the A9D192** range - ** = Amperage of the RCBO

For example for 10A use A9D19210 this is a 2 pole RCBO that can be used on 55 - 0 - 55v AC networks

For more information on the above ranges please see page 2/5 and 2/6 of the attachement

Schneider Electric UK

Attachment(s)

Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.