{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I connect aluminium or copper, flexible or rigid cables to the single and double terminals of the NSX 400 to 630 range.?

In the NSX 400 to 630 range:

Single terminals, part numbers LV432479 or LV432480, can take: aluminium or copper rigid cables with cross-section 35 to 300 mm² and flexible cables with cross-section 240 mm² maximum.

Double terminals, part numbers LV432481 or LV432482, can take: aluminium or copper rigid cables with cross-section 35 to 240 mm² and flexible cables with cross-section 185 mm² maximum.

Schneider Electric UK

Attachment(s)

ghd16312aa.pdfghd16312aa.pdf [788.25 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.