Search FAQs
What is the part number of the cable connecting the LTMR controller and the LTMCU operator control unit?
The LTMCU operator control unit can be connected to the LTMR controller by means of one of the following three cables:
VW3A1104R10 (1m in length)
VW3A1104R30 (3m in length)
VW3A1104R50 (5m in length)
For distances greater than 5 metres, see below:
Released for:Schneider Electric UK
Explore more
Explore more