| FA27969 | How can I obtain the manufacturing date of the Compact NS or NSX circuit-breakers To obtain the manufacturing date of Compact NS or NSX circuit-breakers, read the screen-printed marking at the top of the front panel.
The code P07351,... |
| FA32391 | How many cables per phase can be installed on Ringmaster Ringmaster C (RN2c, RE2c and RN6c)
Up to 2 cables per phase can terminated on Ringmaster C units. Special ECON cable termination kits must be used... |
| FA135827 | I want to download a downlighters / electronic transformer / shaver light instruction manual For Indoor lighting instruction manuals click this link. |
| FA135826 | I want to download Air conditioning / heating / extractor / fan / towel radiators instruction manuals For Air conditioning / heating / extractor / fan / towel radiators instruction manuals click this link. |
| FA135824 | I need information on my air conditioner / dehumidifier For Air conditioning FAQs click this link. |
| FA135825 | I need information on my GET CCTV For GET CCTV FAQs click this link.
|
| FA35358 | How many operations can the circuit breaker do The vacuum circuit breaker (Evolis) used in MCset is capable of 10,000 operations on full load (not full fault current interruption)
The SF6 circuit... |
| FA132878 | What auxiliary voltage is required for my T200E The T200E series 2 will be either 110V ac or 240V ac and will be detailed on the test data sheet inside the cubicle
The T200E series 3 has a voltage... |
| FA86040 | Are spares available for Power Poles (PP18W, PP28W, PP38W)? Yes the following spares are available for Power Poles
PP18KIT - Ceiling Jacking Plate, floor boot, 6 outlet boxes, top shroud, screws and washers... |
| FA86041 | Are spares available for Power Posts (PS1865W, PS2865W)? Yes the following spares are available for Power Posts:
PPTW - Top cover for PS1865W & PS2865W
PPBB - Floor Boot for PS1865W & PS2865W
... |