| FA22920 | Why and when should I use a line choke upstream from an ATV31,ATV312, ATV61, ATV71 variable speed drive? A line choke is used to provide better protection against overvoltages on the line supply and to reduce the harmonic distortion of the current produced... |
| FA142655 | My Drive is showing nSt when I power up and we can not get passed this. nSt can mean a number of different things for different drives and and is dependent on the way they have been set up to operate, therefore we will... |
| FA140105 | Double word or floating point values do not display correctly on an XBTGT, HMISTO, or HMISTU HMI.
If a double word or floating point variable from a PLC displays incorrectly on an XBTGT, HMISTO, or HMISTU HMI, it may be that the double word order... |
| FA86649 | What is the difference between Pressure transmitters, Universal detectors, Pressure switches and Vacuum switches? Pressure transmitters
Are part of a range of products more properly generically referred to as Pressure Transducers. They modify or generate an... |
| FA27996 | What is the purpose of the R1 relay in the ATS01 starters?
The R1 relay output for ATS01 indicates that the motor is being controlled by the soft start and is in a running state. It is a normally open contact... |
| FA28056 | How can I migrate an application from an ATV58 to an ATV71 in PowerSuite? The PowerSuite tool makes it easy to migrate an application from an ATV58 to an ATV71.
To do this, you export the file linked to the ATV58 application... |
| FA86242 | How do I de-mount the circuit breaker in GenieEvo The GenieEvo circuit breaker can be de-mounted and replaced in under 1.5 hours.
Full details of how to de-mount the breaker are on the attached... |
| FA132487 | When you pull out the contactor, do the fuses come attached to the contactor cartridge No, the fuses are not attached to the contactor and remain inside the cubicle when the contactor is withdrawn. |
| FA22753 | How do I set up an ATS01? Potentiometers
There are 3 potentiometers graded from A to E, but not graded in either seconds or Volts, which can be confusing to customers.
Start... |
| FA28050 | What is the principle of PID control seen by ATV variable speed drives? General principle
A PID controller is used to correct the deviation between the reference and the measurement feedback within an acceptable period.... |