Narrow By
  1. Your SelectionRemove All

Standards - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 39

FAQ ID Description
FA243314Do ION7550, ION7650 and ION8800 comply with CoP 1- 2 and 3?
Yes they do, please check the attached certificate
FA132872What is the IP rating of RM6
RM6 has an IP rating of IP3X on the front face and the gas tank is rated at IP67. For more information on RM6 please click here or e-mail: mvswitchgeargb@gb.schneider-electric.com...
FA23919What are the values of the 1P breaking capacities of GV2P circuit-breakers in IT earthing system?
The values below are the breaking capacities of GV2P circuit-breakers operating on an IT earthing system at 400 V 50 Hz, as demonstrated by pole-by-pole...
FA23898How can I cable an Emergency Stop with ATV312 (or ATV31)?
The ATV312 (or ATV31) drive does not have a dedicated safety terminal recognized by the machine safety regulations.   If the machine has to be made...
FA28029What is the difference between a beacon with flashing signals and a beacon with a flash discharge tube?
The light perception of a beacon with Flash discharge tube is different from a beacon with blinking signals. The difference between these two technologies...
FA23719What are the differences between emergency stop and emergency switching-off pushbuttons?
 The Schneider offer includes two types of pushbutton. a) Emergency switching-off with mechanical latching These have direct opening action. The...
FA28044What adaptation parts satisfy standard UL 508 type E on the GV2P and GV3P?
The adaptation parts to be used so that GV2P and GV3P circuit breakers comply with standard UL 508 type E are detailed below. For GV2P circuit breakers: ...
FA28058To what standards do the A class and B class filters correspond in the variable speed drives?
EMC environment and EMC input filter Industrial and commercial EMC environments are described by standards, and Schneider Electric has designed EMC...
FA32998What is the temperature rise level of the GV2Pxx and what does the standard say?
Tests on GV2 circuit breakers are carried out in accordance with IEC 94741, usually in the enclosure because there is a dedicated enclosure. GV2 circuit...
FA136111Does Schneider Electric offer 'safety contactors'?
The term 'safety contactor' does not appear to have any clear definition within the Safety of Machinery standard IEC (BS EN) 60204-1 or within IEC...

Results 1 - 10 of 39