Software Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 37

FAQ ID Description
FA141655Will Zelio Soft 2 V4.5 work on Windows 7 64 bit?
Yes, the only current issue that arises is when it comes to communicate between the PC/Laptop and the Zelio Logic Relay, if you use the USB cable...
FA33574What is the default password for the Sepam relays?
The password for Sepam 20, 40 and 80 is:- 0000 The password for Sepam 2000 is:- 6543210
FA141599How to overcome compatibility issues with EEPROM memory cartridges SR2MEM02 and SR2MEM01?
SR2MEM01   For firmware (software embedded in the Smart Relay) versions ≤ 2.4 It will not work with software versions higher than 2.4   SR2MEM02   For...
FA141555How to check the firmware and hardware version on the Zelio Logic Smart relay?
Check the firmware on the front of the screen (LCD display) of Zelio Smart Relay.     Check the firmware on the software,...
FA141635Can I connect an SR2 or SR3 Zelio Logic Smart Relay to an HMI, separate display screen?
Yes, you can connect the SR2 or SR3 to a small HMI, this HMI comes included in a kit, starter-kit HMISTO & Zelio Logic – reference: VJDSTKSTOSR2 The...
FA142617Will Vijeo Designer work on Windows 7 64 bit?
Yes if the version is V6.0 SP1.1 or higher (like V6.0 SP2.0) Vijeo Designer will work with Windows 7 32 bit also.   Note: You can NOT install V6.0...
FA143924Is ProWORX 32 compatible with Windows 7?
Yes, ProWORX 32 V2.1 with Service Pack 2 is verified for use with Windows 7, 32 or 64 bit (professional version).
FA143923Is it possible to download an application to a PLC using the demo version of Unity software?
Yes, it is possible to download to a PLC with the demo version of Unity provided that you are still within the trial period.
FA143922Is PL7 programming software compatible with 64 bit operating systems?
It is only possible to use PL7 V4.5 SP5 with Windows 7 (64 bit Professional, Enterprise and Ultimate) when used in XP mode.
FA140674SR2 and SR3 LCD display screen not working properly (flashing, strange characters, black screen or stripes).What is wrong with it?
SR2 and SR3   If your Zelio Logic Smart relay screen looks something like this. If you bought your Zelio Smart relay since June 2011 you will have...

Results 1 - 10 of 37