Narrow By
  1. Your SelectionAll

Service and Repair - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 49

FAQ ID Description
FA166807Can I replace the backlight in an XBTGT HMI?
It is possible for a customer to replace the backlight in certain HMIs, but not all of them. The XBTGT5000/6000 and 7000 series HMI backlights can...
FA23067Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?
We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for...
FA23663What are the part numbers of the replacement contact sets for LC1F power contactors?
Spare parts required for each pole of LC1Fxx contactors are as follows:   2 fixed contacts 1 moving contact 2 deflectors 1 backplate ...
FA23690What is the composition of the coded magnetic switches?
The Schneider Electric Coded Magnetic Switch (CMS) is a complete product consisting of two parts: A magnetic switch: this part has a pre wired cable,...
FA22848Are the heads of XY2CDxx trip-wire switches available separately?
Yes, the head for  XY2CDxx trip-wire switches can be ordered as a spare part, number XY2CD01
FA144717What are the differences between 220VAC, 230VAC and 240VAC Mains Supplies and what voltage equipment should I use?
For many years, mainland Western Europe has used a mains electricity supply rated at nominally 220VAC 50Hz. The UK used 240VAC 50Hz.   Currently,...
FA27988Can I replace a broken toggle on an NS / NSX circuit-breaker or switch.
No, the toggle on the breaker frame cannot be replaced as the toggle is integral to the breaker frame. The breaker frame needs to be replaced. However,...
FA23862What is the part number for the SDE contact for a Masterpact NT or NW.
The SDE contact is fitted as a standard on the Masterpact NT or NW circuit breaker. An optional second SDE contact can be fitted to the circuit breaker...
FA23113What should I do if I lose my password on an XBTVA?
If a password is lost on an XBTVA, place a male connector in the XBT's serial link connector. On this male connector, create a link between the following...
FA33169What is the part number of the pushbutton mechanical interlocking device used in the XACA pendant control stations?
The part number of the mechanical interlocking device (mechanism) mounted between two pushbuttons on the XACA pendant control stations is;   XACA009 It...

Results 1 - 10 of 49