| FA28089 | How can I update the firmware of a Twido PLC with the TwidoSoft software? To update the firmware in a Twido PLC with the TwidoSoft software, proceed as follows:
Start TwidoSoft (Start/All programs/TwidoSoft/TwidoSoft),... |
| FA23134 | How can I simulate an application on XBTH, XBTP or XBTE with XBTL1000 without PLC? To simulate an XBTH, XBTP or XBTE application in XBTL1000, without being connected to a PLC, you need to: Deselect the "use the dialogue table" box... |
| FA23867 | What safety functions are available with the XPSMC controller? The XPSMCWIN software is used to configure 30 safety functions on the XPSMC controller.
They are certified in accordance with category 4 of standard... |
| FA27951 | What is the content and what are the advantages of the various "Include" projects installed by default with Vijeo Citect? The "Include" projects installed by default with Vijeo Citect contain predefined elements which can be used in application projects.
"Include" projects... |
| FA22886 | What are the part numbers for cables connecting a PC and a ZELIO PLC? Zelio programmable relays have a special communication port which enables them to be programmed and set up using a PC.
The communication ports on... |
| FA28178 | Is the Zelio Soft software compatible with Windows 7? Zelio Soft software is not compatible with Windows 7. However a new version of zelio soft software will soon be available for use with Windows 7.... |
| FA28106 | Which Magelis terminals are managed by Vijeo Designer Lite? Vijeo Designer Lite configuration software manages the following Magelis terminals:
XBTN200, Terminal equipped with an alphanumeric display... |
| FA28177 | Is TwidoSuite or Twido Soft software compatible with Windows 7? On 6th December 2010 (the date this FAQ was published), TwidoSuite software was not compatible with Windows 7. Twido Soft software will never be compatible... |
| FA23709 | How can I find out the number of remaining authorisations on a group or team software licence? To find out the number of remaining authorisations on a group or team software licence (PL7, Unity, etc.), you can contact one of the following
... |
| FA27958 | How can I edit the Vijeo Citect Variable Tags database in Excel ? To export and handle the Vijeo Citect Variable Tags database in Excel, you need to work on the Variables.dbf file:
Make a copy of this file,... |