| FA133124 | What operating systems are available on the Magelis Smart Industrial PCs? The Operating System on the Magelis Smart and Smart+ is Windows XP Embedded
The operating system is embedded in the device as the Magelis Smart and... |
| FA132990 | What is Unity Application Generator? Deliver your automation projects faster and re-use your know how!
Unity Application Generator (UAG) is an advanced design and generation software... |
| FA132863 | Can I use hit and run Operators can now introduce a time delay between pressing either the Trip or Close buttons and the Recloser or Load Break Switch actual operation... |
| FA132864 | Can I customize the communications settings in WSOS
WSOS can be customised to use different message lengths to suit different communications media. For secure communications (i.e. direct connect) "long"... |
| FA132683 | How is the ICMP Ping utility setup in ConneXview? The ICMP ping control inside of ConneXview has 2 components, one component for discovery of network nodes and another that monitors the node.
See... |
| FA86596 | I have a problem centring labels in the sheet with SYS LABEL Several printers were tested during performance testing of version 3.2.
Solution:
1. Change the printer.
2. The margins can be set to the nearest... |
| FA132314 | How do I configure the IP address of my Ethernet module in PL7 ? If you are using PL7 programming software with an ethernet module (TSXETY4103, TSXETY5103 for Premium, TSXETZ410, TSXETZ510 for Micro) then the number... |
| FA23843 | What is the configuration software for Lexium 05? The configuration software for Lexium 05 servo drives is called Powersuite.
The part number of the PowerSuite software is VW3A8104 and there are... |
| FA23146 | How can I use an Xtel V6.1 application on a PC different from the development PC? You can transfer rights to use the software from one PC to another using the Key manager tool within XTEL. You can use tis tool to transfer rights... |
| FA23098 | How can I manage more than 16 alarms via the dialogue table of an XBT magelis? To have more than 16 alarms, the number of words associated with the alarms must be changed in the dialogue table in order to have the n x 16 alarms... |