Narrow By
  1. Your SelectionAll

Safety - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 97

FAQ ID Description
FA23690What is the composition of the coded magnetic switches?
The Schneider Electric Coded Magnetic Switch (CMS) is a complete product consisting of two parts: A magnetic switch: this part has a pre wired cable,...
FA22954What power supplies should I use to supply light curtains?
Schneider Electric guarantees the correct operation of its light curtains if they are powered with the following modules: ABL8RPS24030: Universal...
FA22755How can I perform the "start test" function on an XUSLA light curtain monitored by an XPSMP configurable module?
Test mode function: This function is neither mandatory nor critical since the XUSLx light curtain has a continuous self-test function (type 4 safety). However,...
FA22714Dynamic periodic monitoring of dual body valves on an XPSPVK eccentric press
Presses used for cold working of metals must be systematically and regularly checked. This check also affects the safety function provided by the...
FA22719Can the XPE on/off foot switches be used to perform an emergency stop function?
No, as due to their mechanical design, there is nothing to prevent an object from getting under the foot switch and preventing actuation of the contact....
FA22712Simulation of a fault on one of the 2 valve flaps (dynamic monitoring) managed by an XPSPVK
The presses used for the cold working of metals must be routinely and regularly checked. This check also affects the safety function provided by...
FA22711What mounting tips can you give for single beam polarised reflex type detectors with the mute function connected to an XPSCM11
Summary of the mute function of an XPSCM Preventa module: The Preventa XPSCM module mute mechanism allows materials to be transported across the...
FA22877What limit switch should I use to monitor the operating direction of a sliding gate?
In order to monitor the operating direction of a sliding gate (detecting movement to the right or to the left) using a single detector, the best solution...
FA163890What are the differences between 380VAC, 400VAC and 415VAC Mains Supplies and what voltage equipment should I use?
For many years, mainland Western Europe has used a mains, 3 phase, electricity supply rated at nominally 380VAC 50Hz. The UK used 415VAC 50Hz.   Currently,...
FA147442What is the recommended maximum spacing between fixings when installing 20mm or 25mm conduit?
Conduit is installed using saddles, spacer bar saddles or quick clip fixings.  The recommended maximum spacing between fixings is 1m.  It is advisable...

Results 11 - 20 of 97