| FA139998 | Can I replace ZB2 parts with ZB4 parts? XB2/ZB2 are the old pushbutton and pilot light range replaced by the current XB4/ZB4 range, also known as Harmony 4 range
By general Telemecanique/Schneider... |
| FA139432 | What replaced XPSAS? What are the differences between XPSAS and the new XPSAF? XPS-AS Replaced by XPS-AF
XPSAS (old model) XPSAF (new model)
XPS-AF has one extra N/O safety... |
| FA139274 | Can the switching half of a coded magnetic switch be bought by itself without the magnet half? No. Although the switched half of the coded magnetic switch often has a number printed on it, it cannot purchased separately. The switch has to be... |
| FA139172 | What replaced XPSAS? What are the differences between XPSAS and the new XPSAK? XPS-AS Replaced by XPS-AK
XPSAS (old model) XPSAK (new model)
XPS-AK has 1 extra N/O... |
| FA137372 | How do I replace a lost or damaged Sphere Controller?
If a Controller is damaged or lost, obtain a replacement and find the record made of the switch settings on the old Controller then duplicate these... |
| FA137239 | Whats the difference between the E251WE & E251BP Converta socket outlets? The only difference is in the way the product is packed. The BP version is blister packed |
| FA27955 | What are the significant differences between the old D2 series contactors and the current Tesys D series? Significant technical changes as follows:
All contactors in the range pre 2001 (D2) required that the auxiliaries be specified in the part number.... |
| FA27953 | What is the possible substitution for XUVH003530 - XUVN0243R? This is an obsolete system comprising an amplifier and interchangeable optical heads for a variety of applications. Such a system no longer exists... |
| FA86241 | What are the advantages of fixed pattern switchgear Fixed pattern switchgear has two major benefits over withdrawable switchgear: -
More compact
Cost effective
For more information on the... |
| FA132878 | What auxiliary voltage is required for my T200E The T200E series 2 will be either 110V ac or 240V ac and will be detailed on the test data sheet inside the cubicle
The T200E series 3 has a voltage... |