Narrow By
  1. Your SelectionAll

Product Substitution - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 70

FAQ ID Description
FA23067Can I convert an XBTL1000 application (XBTF terminal) to Vijeo Designer (XBTGT/GK terminal)?
We have a Services & Projects offer making it easy to migrate XBTL 1000 applications created on XBTF terminals to Vijeo Designer applications for...
FA28074What is the substitution of the GSKC product by the XPSAK module?
The equivalent of the GSKC safety module used for emergency stop monitoring in accordance with standard EN954-1 category 4 is the XPSAK module.  NB: ...
FA23936What stainless steel accessories are available for emergency stop cable pull switches?
The only stainless steel accessories available for emergency stop cable pull switches are the pulley, part number XYCZ708 (X6CR17 ferritic stainless...
FA23032What is an EVERLINK connection and what are its advantages?
TESYS Everlink contactor   TeSys Everlink is an enhancement to Schneider Electric's motor starter solutions, offering combinations of 2 or 3 products...
FA22755How can I perform the "start test" function on an XUSLA light curtain monitored by an XPSMP configurable module?
Test mode function: This function is neither mandatory nor critical since the XUSLx light curtain has a continuous self-test function (type 4 safety). However,...
FA164347What Schneider Electric Drive has replaced the Telemecanique Altivar 58 (ATV58)
The recommended replacement for the ATV58’s are the ATV71’s The list below shows the nearest possible alternatives:  Single Phase Supply 200....240V...
FA164494 What Schneider Electric Drive has replaced the Telemecanique Altivar ATV68
There are two possible replacements as the ATV68 could be used on High Torque applications or on Standard Torque applications so listed below are...
FA163890What are the differences between 380VAC, 400VAC and 415VAC Mains Supplies and what voltage equipment should I use?
For many years, mainland Western Europe has used a mains, 3 phase, electricity supply rated at nominally 380VAC 50Hz. The UK used 415VAC 50Hz.   Currently,...
FA164455What Schneider Electric Drive has replaced the Telemecanique Altivar ATV66
There are two possibilities due to the fact the ATV66 could be used as a Constant Torque or a Variable Torque drive. So the application the drive...
FA164348What Schneider Electric Drive has replaced the Telemecanique Altivar ATV28
The drive that replaced the ATV28 range was the ATV31 range which has its self been replaced in most cases by the ATV312 range. Below is a list of...

Results 1 - 10 of 70