| FA137230 | Does the 56 series product include the surface mount enclosure? If the part number includes LE (Less enclosure) you will need to order the appropriate 56 series surface mount enclosure for the product. An example... |
| FA135938 | What are the recommended fuse link replacements for Twinbreak / Quadbreak? |
| FA136067 | I would like more information on Floor boxes Please find below a link to the Floor box catalogue including range information, technical description and dimensions. |
| FA133184 | Can I mount an LR97D electronic over current relay on DIN rail? Yes, the LR97D can be mounted on DIN rail using the LAD7B106 Terminal Block
|
| FA23670 | What pushbutton family is recommended for installation with a 9001K type station? For an installation with empty boxes/enclosures of the 9001KY, KYS and SKY type, the recommended family of 30 diameter buttons is 9001K.
More information... |
| FA132878 | What auxiliary voltage is required for my T200E The T200E series 2 will be either 110V ac or 240V ac and will be detailed on the test data sheet inside the cubicle
The T200E series 3 has a voltage... |
| FA132875 | Can I use a fibre optic network to communicate with my T200 Yes a fibre optic communications network can be used with your T200I/E. A fibre optic converter will need to be installed inside the cubicle and plugged... |
| FA132869 | Can I install an RM6 cubicle outside RM6 can be installed in an outdoor installation but will required an outdoor cabinet for additional IP protection.
For more infomation on RM6 please... |
| FA132868 | Can a recloser be controlled remotely Yes when connected to a communications network via a modem, a recloser or load break switch/sectionaliser can be controlled remotely.
For more information... |
| FA132488 | Can Motorpact be supplied as a stand-alone or incorporated into a switchboard Motorpact can be supplied for both: -
Stand-alone on all starting methods
Part of a switchboard with GenieEvo or MCset
For more details... |