| FA23735 | Where should I connect the SZ1RV1202 potentiometer (pot) to the ATV variable speed drives? The potentiometer part number: SZ1RV1202 must be connected to one of the 0...10 V analog inputs on ATVxxxx range variable speed drives:
ATV12... |
| FA28095 | What are the part numbers of the BA9S type bulbs for XB4/XB5 pushbutton controls? For Harmony XB4/XB5 22 diameter control and signalling units, whether: LED lamps, incandescent lamps, neon lamps, there are part numbers with BA9s... |
| FA24940 | Do the GS1 or GS2 disconnect switches come with fuses? No, because the fuse is linked to the application, eg:
fast-acting semi-conductor fuses for electronic loads
aM fuses for motor loads
... |
| FA23920 | What is the operation of the GV2AD fault signalling contacts of the GV2 circuit-breakers? GV2ME, GV2P, GV2L, GV2LE, GV3P and GV3L circuit-breakers can be fitted with the following optional fault indicating contact blocks:
GVAD0110
GVAD0101... |
| FA23663 | What are the part numbers of the replacement contact sets for LC1F power contactors? Spare parts required for each pole of LC1Fxx contactors are as follows:
2 fixed contacts
1 moving contact
2 deflectors
1 backplate
... |
| FA23278 | In what type of control station can I install control and signaling units from the Harmony style 5 range? Harmony style 5 range (XB5) buttons can be used on the front panel of the following control stations:
XALK, XALD: plastic control stations,
... |
| FA23212 | Is "remote reset" function available for GV2 / GV3 / GV7 circuit breakers? No remote reset is available for GV2/GV3/GV7 circuit breakers. Remote tripping, using shunt trips, is available but no reset.
Remote resets are... |
| FA22942 | Where can I find the characteristics of the LC1D contactors? You will find all the characteristics of LC1Dxx contactors on the Tesys web page:
The section Downloads has documents ( Catalogues, Brochures, Catalogue... |
| FA23032 | What is an EVERLINK connection and what are its advantages? TESYS Everlink contactor
TeSys Everlink is an enhancement to Schneider Electric's motor starter solutions, offering combinations of 2 or 3 products... |
| FA22954 | What power supplies should I use to supply light curtains? Schneider Electric guarantees the correct operation of its light curtains if they are powered with the following modules:
ABL8RPS24030: Universal... |