| FA23873 | Can I access the diagnostics of an OTB island using the Advantys software? No, there are no diagnostic functions for an OTB island in the Advantys software.
The OTB NIM modules manage a limited number of online operations,... |
| FA22755 | How can I perform the "start test" function on an XUSLA light curtain monitored by an XPSMP configurable module? Test mode function: This function is neither mandatory nor critical since the XUSLx light curtain has a continuous self-test function (type 4 safety).
However,... |
| FA141655 | Will Zelio Soft 2 V4.5 work on Windows 7 64 bit?
Yes, the only current issue that arises is when it comes to communicate between the PC/Laptop and the Zelio Logic Relay, if you use the USB cable... |
| FA141555 | How to check the firmware and hardware version on the Zelio Logic Smart relay?
Check the firmware on the front of the screen (LCD display) of Zelio Smart Relay.
Check the firmware on the software,... |
| FA142621 | What address to use for TSXETZ410 and TSXETZ510? Set an address of a TSXETZ410 and TSXETZ510. This FAQ is to alert users NOT to set the IP address on any of theses devices of 255.255.255.255.
Do not use this IP address, there is a risk of becoming... |
| FA142617 | Will Vijeo Designer work on Windows 7 64 bit? Yes if the version is V6.0 SP1.1 or higher (like V6.0 SP2.0)
Vijeo Designer will work with Windows 7 32 bit also.
Note: You can NOT install V6.0... |
| FA142642 | How to connect XPSMC via USB, using TSXCUSB485 USB converter?
XPSMC + TSXCUSB485 hardware connection
XPSMC + TSXCUSB485 software rules
|
| FA140674 | SR2 and SR3 LCD display screen not working properly (flashing, strange characters, black screen or stripes).What is wrong with it? SR2 and SR3
If your Zelio Logic Smart relay screen looks something like this.
If you bought your Zelio Smart relay since June 2011 you will have... |
| FA35830 | Question Why does the Sepam Series 20, 40 and 80 Relay not display waveforms for all phases of current / voltage? When certain variables are calculated rather than acquired (measured) by Sepam, the waveform associated to those variables is not available. Those... |
| FA35833 | How to retrieve a fault recording (OPG) in SFT2841 from the Sepam Series 20, 40 and 80 Relay? Steps to retrieve fault recording in SFT2841:
(Note: Screen Caps may appear differently depending on Sepam series)
1. Verify communication between... |