| FA23849 | How do I wire the different elements of an XVB signal tower? Principle: The terminal numbers correspond to the location of the illuminated lens unit: Example: To illuminate lens unit number 4 , terminals... |
| FA23896 | Are the Zelio Relay (RU, RX) plug-in relays interchangeable with the old RH range of plug in relay bases? No, installing Zelio Relay (RU, RX) plug-in relays in to a base from the RH range is not possible, both relay and base should be replaced with the... |
| FA23826 | How many terminal shields do the GS1AP part numbers contain? Part numbers GS1AP33, GS1AP43 and GS1AP63 are terminal shields for 3-pole fuse switch disconnectors.
GS1AP33 for 100 - 160A rating
GS1AP43 for ... |
| FA23212 | Is "remote reset" function available for GV2 / GV3 / GV7 circuit breakers? No remote reset is available for GV2/GV3/GV7 circuit breakers. Remote tripping, using shunt trips, is available but no reset.
Remote resets are... |
| FA23069 | How can manual override of an automatic control system be implemented? There are many instances where it is necessary to have automatic control of a motor and also the provision of a manual override.
A typical... |
| FA22878 | What is the tripping class of the GV2 ME, GV2 P and GV2 RT? The tripping class for GV2MExx, GV2Pxx, GV2RTxx circuit-breakers is class 10. Class 10 corresponds to a direct on-line motor starting time between... |
| FA22893 | What are the differences between the various tripping classes of thermal overload? There are four classes of thermal overload relay:
10A
10
20
30
These class numbers indicate the trip characteristics from cold state, and should be... |
| FA22848 | Are the heads of XY2CDxx trip-wire switches available separately? Yes, the head for XY2CDxx trip-wire switches can be ordered as a spare part, number XY2CD01 |
| FA165720 | Do you have a touch up paint for the iline panel board? We can supply an aerosol spray paint, part number SDPAINT |
| FA164490 | What are the maximum permitted loads in Watts for multiple electronic dimmer modules in a single enclosure?
Front plate gang size
2
3
4
6
8
9
... |