| FA23058 | How can I import an OTB CANopen island communicating with an M340 in the Unity software?
Before importing an OTB CANopen island, the ".DCF" file must first be generated using the Advantys software as follows:
Then in Unity, proceed... |
| FA23873 | Can I access the diagnostics of an OTB island using the Advantys software? No, there are no diagnostic functions for an OTB island in the Advantys software.
The OTB NIM modules manage a limited number of online operations,... |
| FA22914 | Is it possible to install a contactor downstream from a variable speed drive? It is possible to install a contactor downstream of a variable speed drive but this involves a high risk of damage to the equipment if the contactor... |
| FA23075 | Can I install a potentiometer, part number SZ1RV1202, in an XACA enclosure? No. There are two reasons preventing a potentiometer, part number SZ1RV1202, from being installed in an XACA enclosure:
1. An SZ1RV1202 potentiometer... |
| FA22870 | How can Schneider Electric Soft Starts be used to run three phase motors in both direction(Forwards and Reverse) Soft Starters can not reverse the direction of the motor. To achieve reversal of the motor’s direction a set of reversing contactors must be wired... |
| FA22750 | What is the part number for a potentiometer to control Schneider Electric Altivar variable speed drives (VSDs) ? The recommended specification for potentiometers compatible across our range of drives (ATV11, ATV12, ATV31, ATV312, ATV21, ATV61 and ATV71 and the legacy... |
| FA28149 | Does Schneider Electric have a solid state relay offer? Schneider Electric offers a range of solid state relays.
The Schneider Electric SSR solid state relays have the following benefits over electromechanical... |
| FA24894 | Can I use a "conventional" limit switch for safety applications? Yes, it is possible to use a "conventional" limit switch for safety applications, as long as the switch is "positive action"
Definition of positive... |
| FA23936 | What stainless steel accessories are available for emergency stop cable pull switches? The only stainless steel accessories available for emergency stop cable pull switches are the pulley, part number XYCZ708 (X6CR17 ferritic stainless... |
| FA24940 | Do the GS1 or GS2 disconnect switches come with fuses? No, because the fuse is linked to the application, eg:
fast-acting semi-conductor fuses for electronic loads
aM fuses for motor loads
... |