Hardware Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 73

FAQ ID Description
FA23075Can I install a potentiometer, part number SZ1RV1202, in an XACA enclosure?
No. There are two reasons preventing a potentiometer, part number SZ1RV1202, from being installed in an XACA enclosure: 1. An SZ1RV1202 potentiometer...
FA246418Is the full function test Kit (33595) a complete kit?
The 33595 is a complete test kit for NW& NT with micrologic trip unit, NS with STR and micrologic tip unit, however it comes with a non uk power plug...
FA243862On the Prisma P range, does the part number 08676 allows mounting 1 or 2 fans?
This roof was redesigned in 2014. In old catalogues you will find the version that was sold back then, and that one allowed 2 fans. The current one...
FA241834What micrologic trip unit comes with the standard MGP6303X & MGP4003X moulded case breakers?
The MGP6303x, MGP6304X, MGP4003X, & MGP4004X moulded case circuit breakers come with Micrologic 2.3 fitted as standard. The MGP4003X5E, MGP4004X5E,...
FA32985What is the difference between a VPIS and a VDS (SM6, RM6 power ON pilot light)?
VPIS (Voltage Presence Indicator System): According to standard IEC 61958 the purpose of a VPIS is to signal a voltage presence. If a lamp is unlit,...
FA132312What is the difference between a TSXETZ410 & TSXETZ510 Ethernet gateway?
The TSX ETZ 510 offers exactly the same functionality as the TSXETZ410 with the addition of  8 Mbytes reserved for users web site.
FA141655Will Zelio Soft 2 V4.5 work on Windows 7 64 bit?
  Yes, the only current issue that arises is when it comes to communicate between the PC/Laptop and the Zelio Logic Relay, if you use the USB cable...
FA141635Can I connect an SR2 or SR3 Zelio Logic Smart Relay to an HMI, separate display screen?
Yes, you can connect the SR2 or SR3 to a small HMI, this HMI comes included in a kit, starter-kit HMISTO & Zelio Logic – reference: VJDSTKSTOSR2   The...
FA142680What equipment uses the TSXCUSB485 USB converter?
Here are some of our products that use this USB converter:   XPSMC             safety modules TSX Micro        PLC’s Premium           PLC’s Atrium             PLC’s M238               PLC’s Twido              PLC’s XBT...
FA27937What is the cabling diagram for the SR1CBL01 cable?
To be able to connect first generation Zelio programmable relays (part number SR 1xx) to a PC supporting the ZelioSoft programming software (part...

Results 1 - 10 of 73