| FA142617 | Will Vijeo Designer work on Windows 7 64 bit? Yes if the version is V6.0 SP1.1 or higher (like V6.0 SP2.0)
Vijeo Designer will work with Windows 7 32 bit also.
Note: You can NOT install V6.0... |
| FA142669 | Did the appearance of Tesys D contactors and control relays change? What changed on the “looks” for LC1D contactors (sizes LC1D09 to LC1D38) and CAD control relays? Yes, there is an evolution happening during the 2nd quarter of 2012, in which will change slightly their appearance.
This change will affect the Tesys... |
| FA142680 | What equipment uses the TSXCUSB485 USB converter?
Here are some of our products that use this USB converter:
XPSMC safety modules
TSX Micro PLC’s
Premium PLC’s
Atrium PLC’s
M238 PLC’s
Twido PLC’s
XBT... |
| FA142687 | What is the difference between an LUB12 32 & LUB120 320 Tesys U starter?
The Tesys U non reversing starter controller offers two types of power base units in its range
LUB12 & LUB120 (0 – 12A, 5.5kw at 400V)
LUB32 & LUB320... |
| FA143924 | Is ProWORX 32 compatible with Windows 7? Yes, ProWORX 32 V2.1 with Service Pack 2 is verified for use with Windows 7, 32 or 64 bit (professional version). |
| FA143923 | Is it possible to download an application to a PLC using the demo version of Unity software? Yes, it is possible to download to a PLC with the demo version of Unity provided that you are still within the trial period. |
| FA143922 | Is PL7 programming software compatible with 64 bit operating systems? It is only possible to use PL7 V4.5 SP5 with Windows 7 (64 bit Professional, Enterprise and Ultimate) when used in XP mode. |
| FA141939 | What replaced Integral 18 and 32 DOL starters - LD1, LD3, LD4, LB1 and LB6? Integral Replaced by Tesys U
Integral 18 and Integral 32 DOL (old model) Tesys U - LUB (new model)
... |
| FA141913 | What can I use to replace DOL Integral 18 and 32, LD1, LD3 and LD4? Can I replace Integral 18 and 32 using contactors and MCB’s? Yes, you can, using the kit we have prepared:
Integral 18 and Integral 32 replaced by LC1D+GV2
New kit, using contactors Tesys D LC1D + MCB’s... |
| FA141941 | What replaced Integral 18 and 32 DOL reversing starters – LD5, LB1 and LB6? What replaced Integral 18 and 32 DOL reversing starters – LD5, LB1 and LB6?
Integral Replaced by Tesys U
Integral 18 and 32 reversing DOL (old... |