Compatibility - FAQs

FAQ Search
Most Recently Published FAQs

Results 11 - 20 of 100

FAQ ID Description
FA141655Will Zelio Soft 2 V4.5 work on Windows 7 64 bit?
Yes, the only current issue that arises is when it comes to communicate between the PC/Laptop and the Zelio Logic Relay, if you use the USB cable...
FA144717What are the differences between 220VAC, 230VAC and 240VAC Mains Supplies and what voltage equipment should I use?
For many years, mainland Western Europe has used a mains electricity supply rated at nominally 220VAC 50Hz. The UK used 240VAC 50Hz.   Currently,...
FA33574What is the default password for the Sepam relays?
The password for Sepam 20, 40 and 80 is:- 0000 The password for Sepam 2000 is:- 6543210
FA141633What replaced XPSAPF? What are the differences between XPSAPF and the new XPSAR?
XPS-APF replaced by XPS-AR  XPSAPF (old model)                                                    XPSAR (new model) XPS-AR has 2 extra solid...
FA141599How to overcome compatibility issues with EEPROM memory cartridges SR2MEM02 and SR2MEM01?
SR2MEM01   For firmware (software embedded in the Smart Relay) versions ≤ 2.4 It will not work with software versions higher than 2.4   SR2MEM02   For...
FA141555How to check the firmware and hardware version on the Zelio Logic Smart relay?
Check the firmware on the front of the screen (LCD display) of Zelio Smart Relay.     Check the firmware on the software,...
FA141635Can I connect an SR2 or SR3 Zelio Logic Smart Relay to an HMI, separate display screen?
Yes, you can connect the SR2 or SR3 to a small HMI, this HMI comes included in a kit, starter-kit HMISTO & Zelio Logic – reference: VJDSTKSTOSR2 The...
FA141863What replaced XPSCE? What are the differences between XPSCE and the new XPSCM?
XPS-CE Replaced by XPS-CM   XPSCE (old model)                                                       XPSCM (new model) XPS-CM has 3 extra solid...
FA141670What replaced XPSASF? What are the differences between XPSASF and the new XPSAK?
XPS-ASF Replaced by XPS-AK   XPSAFS (old model)                                                    XPSAK (new model) XPS-AK has one extra N/O...
FA142425Is there an enclosure for GV3, to make an enclosed starter? Can we fit GV3P, GV3L and GV3ME? Can we mount LC1 contactor?
Yes, there is an enclosure that can take the new GV3P and GV3L, plus there’s space to mount a contactor inside. The new enclosures GV3PC aren’t suitable...

Results 11 - 20 of 100