Narrow By
  1. Your SelectionAll

Commercial - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 33

FAQ ID Description
FA23926What is the meaning of the utilization categories AC1 and AC3 for the Tesys contactors?
The standard utilization categories defines the current making and breaking values for contactors. They depend on the following: The type of...
FA23032What is an EVERLINK connection and what are its advantages?
TESYS Everlink contactor   TeSys Everlink is an enhancement to Schneider Electric's motor starter solutions, offering combinations of 2 or 3 products...
FA141635Can I connect an SR2 or SR3 Zelio Logic Smart Relay to an HMI, separate display screen?
Yes, you can connect the SR2 or SR3 to a small HMI, this HMI comes included in a kit, starter-kit HMISTO & Zelio Logic – reference: VJDSTKSTOSR2 The...
FA141801Where to get drivers for the Bluetooth adaptor VW3A8115 for Zelio Logic Smart Relay SR2/SR3/Twido/ATV?
The drivers are contained in the CD, included in the Bluetooth adaptor kit accompanies, those drivers are also obtainable here. Bluetooth adaptor...
FA142019Can I get the magnet or the detector of a Coded Magnetic Switch XCS for Safety, as separate component?
No, the Safety coded magnetic switches have to be bought as a pair, which will include the magnet and the detector. Note: Other variations on...
FA142617Will Vijeo Designer work on Windows 7 64 bit?
Yes if the version is V6.0 SP1.1 or higher (like V6.0 SP2.0) Vijeo Designer will work with Windows 7 32 bit also.   Note: You can NOT install V6.0...
FA142669Did the appearance of Tesys D contactors and control relays change? What changed on the “looks” for LC1D contactors (sizes LC1D09 to LC1D38) and CAD control relays?
Yes, there is an evolution happening during the 2nd quarter of 2012, in which will change slightly their appearance. This change will affect the Tesys...
FA141939What replaced Integral 18 and 32 DOL starters - LD1, LD3, LD4, LB1 and LB6?
Integral Replaced by Tesys U   Integral 18 and Integral 32 DOL (old model)                                          Tesys U - LUB (new model)                                ...
FA141913What can I use to replace DOL Integral 18 and 32, LD1, LD3 and LD4? Can I replace Integral 18 and 32 using contactors and MCB’s?
Yes, you can, using the kit we have prepared:   Integral 18 and Integral 32 replaced by LC1D+GV2 New kit, using contactors Tesys D LC1D + MCB’s...
FA141941What replaced Integral 18 and 32 DOL reversing starters – LD5, LB1 and LB6?
What replaced Integral 18 and 32 DOL reversing starters – LD5, LB1 and LB6?   Integral Replaced by Tesys U   Integral 18 and 32 reversing DOL (old...

Results 1 - 10 of 33