| FA36149 | How many samples per cycle are captured for the Sepam Series 20, 40 and 80? How many samples are used for protection, measurement, and waveform display? The Sepam protection relay samples at 36 samples per cycle to calculate true RMS values for displayed phase current and overload protection. It can... |
| FA135938 | What are the recommended fuse link replacements for Twinbreak / Quadbreak? |
| FA135995 | I need an instruction leaflet for Exclusive Decorative / Moulded or Ultimate Flat Plate / Moulded Rotary dimmer Please find the instructions below |
| FA22997 | What are the recommended characteristics for a Modbus Jbus RS485 / Com / ABT network cable? The recommended characteristics of the RS485/Modbus cable are: twisted pair with tinned copper braid shielding. Minimum overlap: 65%. Gauge: AWG 24.... |
| FA22704 | How many sensors can I place on the temperature inputs T1 and T2 of a LTMR motor management controller? The motor temperature is monitored via an LTMR motor management controller using PTC (or NTC) sensors installed on the motor coils.
The motors generally... |
| FA23113 | What should I do if I lose my password on an XBTVA? If a password is lost on an XBTVA, place a male connector in the XBT's serial link connector.
On this male connector, create a link between the following... |
| FA133184 | Can I mount an LR97D electronic over current relay on DIN rail? Yes, the LR97D can be mounted on DIN rail using the LAD7B106 Terminal Block
|
| FA132167 | The data being displayed on the PM700 Power Meter is inaccurate or not what I expect? 1.
Possible Cause
Incorrect setup values
Possible Solution
Check that the correct values have been entered for the power meter setup parameters -... |
| FA132169 | I cannot communicate with a Power Meter (PM710 or PM750) from a remote personal computer? 1.
Possible Cause
The Power Meter address is incorrect
Possible Solution
Check that the Power Meter is correctly addressed
2.
Possible Cause
Power... |
| FA132168 | The display is blank after applying power to a PM700 Power Meter? 1.
Possible Cause
The Power Meter may not be receiving the necessary power. If the Power Meters power terminals are daisy chained ensure that the... |