| FA139172 | What replaced XPSAS? What are the differences between XPSAS and the new XPSAK? XPS-AS Replaced by XPS-AK
XPSAS (old model) XPSAK (new model)
XPS-AK has 1 extra N/O... |
| FA137893 | What does H29 on the end of a part number indicate? Certain products across the Schneider Electric range have features that are particular to specific country or language.
To enable differentiation of products... |
| FA138197 | How do I work out what a 9012G or 9016G range pressure switch is from the part number The part number for a 9012G and 9016G is made up from the following table
Note
Electrical Connections : 1/2”-14 NPTF, PG13.5, or ISO M20. For metric... |
| FA138031 | How do I wire up an LE1GBK starter? An overload must first be fitted beneath the contactor. It will require a K series overload ( part numbers LR2K03**)
POWER WIRING
The 3 incoming phases... |
| FA136856 | What are the separate parts required to build up star delta starters for motors 7.5kW through to 132kW suitable for mounting on DIN rail? The table below indicates the selection of the power switching components necessary to build up a star delta starters, with mechanical interlocks... |
| FA137116 | Where can I find a copy of the Smart Wireless Lighting User Guide? The Guide can be downloaded below |
| FA137117 | Where can I find a copy of the Sphere Wireless Lighting Instruction Manual? The Instruction Manual can be downloaded below |
| FA23248 | Can I connect a PTC probe to an ATV11, ATV12 , ATV21, ATV312 , ATV31, ATV32, ATV61 or ATV71 variable speed drive? IF YOU ARE USING ANY OF THE DRIVES IN A ATEX AREA YOU CANNOT USE THE
PTC INPUT OF THE DRIVE YOU MUST USE AN ATEX APPROVED UNIT
ATV11, ATV12 and... |
| FA32031 | Is two way / intermediate control achievable using Electronic Dimmers?
For 2 Way or Multi-Way installations, separate momentary action ‘retractive’ press switches are required. Any existing 2 way or intermediate switches... |
| FA86407 | What types of terminal blocks are available for the Sepam Relay? The Sepam Series 20, 40 & 80 base units are available with 2 different types of terminal blocks: Screw Type (CCA620) & Ring Lugs (CCA622).
Relays... |