Narrow By
  1. Your SelectionAll

Cabling and Connection - FAQs

FAQ Search
Most Recently Published FAQs

Results 31 - 40 of 100

FAQ ID Description
FA27988Can I replace a broken toggle on an NS / NSX circuit-breaker or switch.
No, the toggle on the breaker frame cannot be replaced as the toggle is integral to the breaker frame. The breaker frame needs to be replaced. However,...
FA24980How can I solve an OBF fault on ATV58?
If the drive indicates the OBF fault  it is caused by over braking. This is caused when the drive's DC bus voltage exceeds the permitted voltage...
FA33584Is top cable entry available on Ringmaster
Yes top entry is available on Ringmaster C and Ringmaster Range. More details on Ringmaster C or Ringmaster range.
FA27982Can I fit a CT module and a residual current module (vigi) onto the Compact NSX MCCB range.
No, a CT module cannot be fitted onto a residual current module (vigi) from  the Compact NSX MCCB range.
FA24973What is the ohmic tripping value of a PTC probe on an ATV58?
The motor temperature is detected by PTC probes connected to the ATV58 drive via specific inputs (+10, AI3A, AI3B and COM) on extension card VW3A58201.   The...
FA27970What is the meaning of the terms 2P2d, 3P3d, 4P3d, 4P4d, 4P3d+N/2 and 4P3d+OSN on the Compact NSX circuit-breaker trip units.
The first number corresponds to the number of poles. The second number corresponds to the number of protected poles. The first letter stands for Pole. The...
FA27986Can I connect aluminium or copper, flexible or rigid cables to the single and double terminals of the NSX 400 to 630 range.
In the NSX 400 to 630 range: Single terminals, part numbers LV432479 or LV432480, can take: aluminium or copper rigid cables with cross-section 35...
FA141626What replaced XPSAPF? What are the differences between XPSAPF and the new XPSAK?
XPS-APF Replaced by XPS-AK   XPSAPF (old model)                                                                 XPSAK (new model) XPS-AK...
FA141633What replaced XPSAPF? What are the differences between XPSAPF and the new XPSAR?
XPS-APF replaced by XPS-AR  XPSAPF (old model)                                                    XPSAR (new model) XPS-AR has 2 extra solid...
FA141635Can I connect an SR2 or SR3 Zelio Logic Smart Relay to an HMI, separate display screen?
Yes, you can connect the SR2 or SR3 to a small HMI, this HMI comes included in a kit, starter-kit HMISTO & Zelio Logic – reference: VJDSTKSTOSR2 The...

Results 31 - 40 of 100