Narrow By
  1. Your SelectionAll

Cabling and Connection - FAQs

FAQ Search
Most Recently Published FAQs

Results 1 - 10 of 100

FAQ ID Description
FA22857 What is the pin-out of the RJ45 socket of an ATV31 for connection of Modbus, CanOpen and PowerSuite cables
     The RJ45 socket of the ATV31 can be used for connection to the following networks and accessories:      a PLC via a Modbus bus or via a CANopen...
FA164663Is it possible to program a Twido PLC through the 499TWD01100 TwidoPort Ethernet TCP/IP interface module?
Yes it is possible to program a Twido PLC via the TwidoPort Ethernet interface module. When configuring an Ethernet connection to a PC in TwidoSuite,...
FA166803How do I configure the IP address in a 499TWD01100 TwidoPort TCP/IP communications module?
The IP address of a TwidoPort Ethernet interface is stored in the Twido PLC using TwidoSuite software.  This means that the TwidoPort can then be...
FA22920Why and when should I use a line choke upstream from an ATV31,ATV312, ATV61, ATV71 variable speed drive?
A line choke is used to provide better protection against overvoltages on the line supply and to reduce the harmonic distortion of the current produced...
FA23075Can I install a potentiometer, part number SZ1RV1202, in an XACA enclosure?
No. There are two reasons preventing a potentiometer, part number SZ1RV1202, from being installed in an XACA enclosure: 1. An SZ1RV1202 potentiometer...
FA23735Where should I connect the SZ1RV1202 potentiometer (pot) to the ATV variable speed drives?
The potentiometer part number: SZ1RV1202 must be connected to one of the 0...10 V analog inputs on ATVxxxx range variable speed drives: ATV12...
FA22870How can Schneider Electric Soft Starts be used to run three phase motors in both direction(Forwards and Reverse)
   Soft Starters can not reverse the direction of the motor. To achieve reversal of the motor’s direction a set of reversing contactors must be wired...
FA22750What is the part number for a potentiometer to control Schneider Electric Altivar variable speed drives (VSDs) ?
The recommended specification for potentiometers compatible across our range of drives (ATV11, ATV12, ATV31, ATV312, ATV21, ATV61 and ATV71 and the legacy...
FA28074What is the substitution of the GSKC product by the XPSAK module?
The equivalent of the GSKC safety module used for emergency stop monitoring in accordance with standard EN954-1 category 4 is the XPSAK module.  NB: ...
FA23936What stainless steel accessories are available for emergency stop cable pull switches?
The only stainless steel accessories available for emergency stop cable pull switches are the pulley, part number XYCZ708 (X6CR17 ferritic stainless...

Results 1 - 10 of 100