FAQs

FAQ Search
Most Recently Published FAQs

Results 51 - 60 of 100

FAQ ID Description
FA23278In what type of control station can I install control and signaling units from the Harmony style 5 range?
Harmony style 5 range (XB5) buttons can be used on the front panel of the following control stations: XALK, XALD: plastic control stations, ...
FA23212Is "remote reset" function available for GV2 / GV3 / GV7 circuit breakers?
No remote reset  is available for GV2/GV3/GV7 circuit breakers. Remote tripping, using shunt trips, is available but no reset. Remote resets are...
FA23716Are the XCSDMCx7 coded magnetic switches with contact and LED compatible with the XPSAK or XPSAR Preventa modules?
No, the XCSDMCx7 coded magnetic switches are not compatible, however other Preventa Safety modules are as detailed below: Coded magnetic switches:   ...
FA23690What is the composition of the coded magnetic switches?
The Schneider Electric Coded Magnetic Switch (CMS) is a complete product consisting of two parts: A magnetic switch: this part has a pre wired cable,...
FA22942Where can I find the characteristics of the LC1D contactors?
You will find all the characteristics of LC1Dxx contactors on the Tesys web page:   The section Downloads has documents ( Catalogues, Brochures, Catalogue...
FA23069How can manual override of an automatic control system be implemented?
There are many instances where it is necessary to have automatic control of a motor and also the provision of a manual override.   A typical...
FA23032What is an EVERLINK connection and what are its advantages?
TESYS Everlink contactor   TeSys Everlink is an enhancement to Schneider Electric's motor starter solutions, offering combinations of 2 or 3 products...
FA22954What power supplies should I use to supply light curtains?
Schneider Electric guarantees the correct operation of its light curtains if they are powered with the following modules: ABL8RPS24030: Universal...
FA22755How can I perform the "start test" function on an XUSLA light curtain monitored by an XPSMP configurable module?
Test mode function: This function is neither mandatory nor critical since the XUSLx light curtain has a continuous self-test function (type 4 safety). However,...
FA22878What is the tripping class of the GV2 ME, GV2 P and GV2 RT?
The tripping class for GV2MExx, GV2Pxx, GV2RTxx circuit-breakers is class 10. Class 10 corresponds to a direct on-line motor starting time between...

Results 51 - 60 of 100