Search FAQs
Can the class 20 LRD15** thermal overloads be used with LC1D38** contactors?
Yes, although the LRD15** overload setting range only goes up to 32 amps you can fit any one of these overloads to an LC1D38** contactor.
The LC1D38** contactor shares the same frame body as the LC1D25** and the LC1D32** contactors.
Note that there are alternatives in the new range, which allow setting ranges to cover most of the Tesys D range. See the attached catalogue extract for further information.
** = Coil voltage code in the case of contactors, and digits representing current setting range in the case of thermal overloads
The LC1D38** contactor shares the same frame body as the LC1D25** and the LC1D32** contactors.
Note that there are alternatives in the new range, which allow setting ranges to cover most of the Tesys D range. See the attached catalogue extract for further information.
** = Coil voltage code in the case of contactors, and digits representing current setting range in the case of thermal overloads
Released for:Schneider Electric UK
Attachment(s)
Explore more
Explore more