Search FAQs
Is XACA069SPEC0712 available to buy?
XACA069SPEC0712 Pendant was a custom build specification for RS Components.
This pendant is no longer available as it originally contained a unique contact block (ZA2BZ141) which is no longer manufactured and has no replacement.
ZA2BZ141 contact block contained 3 contacts of 2 N/C + 1 N/O configuration. There is no method for replicating this configuration with individual contacts, as only 2 contacts may be associated with any one pushbutton in an XACA pendant.
Whilst it is not possible to create a like for like replacement in the XACA range of pendants, a build of the same function can be created in the XACB range, as this can replicate the ZA2BZ141 function using Harmony 5 components, which cannot be used in the XACA pendants.
Please note:
Please note:
Although there is physical space in the enclosure, the declaration of conformity for XACB range does not include Harmony 5 components (ZB5 / XB5). Only those contacts associated with the range in the catalogue are listed. You can find the declaration of conformity on www.se.com.
There is a major difference in the Shock resistance to IEC 60068-2-27 between the XACA Pendents and associated buttons and the XB5 Harmony range, the Harmony XB5 range has a very good but significantly lower shock rating.
There is a major difference in the Shock resistance to IEC 60068-2-27 between the XACA Pendents and associated buttons and the XB5 Harmony range, the Harmony XB5 range has a very good but significantly lower shock rating.
XB5 Harmony conforms to
30 gn (duration = 18 ms) for half sine wave acceleration conforming to IEC 60068-2-27
50 gn (duration = 11 ms) for half sine wave acceleration conforming to IEC 60068-2-27
50 gn (duration = 11 ms) for half sine wave acceleration conforming to IEC 60068-2-27
XACA Harmony conforms to
Shock resistance 100 gn conforming to IEC 60068-2-27
A scheme sheet with a parts listing for self assembly is attached for download, however although these parts fit Schneider Electric cannot guarantee the application because of the declaration of conformity and shock resistance issue detailed above.
Released for:Schneider Electric UK
Attachment(s)
Explore more
Explore more