Search FAQs
How do I configure the IP address in a 499TWD01100 TwidoPort TCP/IP communications module?
The IP address of a TwidoPort Ethernet interface is stored in the Twido PLC using TwidoSuite software. This means that the TwidoPort can then be replaced without the need for configuration.
To assign an IP address, follow the steps below;
Select the ‘describe’ tab in TwidoSuite, then choose the appropriate PLC and Ethernet interface (this can be found in the hardware catalogue under ‘Network elements’, then ‘Modbus elements’).
Double click on the Ethernet Interface module and set the required IP address and gateway address (the mac address should be 255.255.255.0).
Double click on the serial port of the PLC and set it as Modbus (address 1 in this example). Link the Ethernet interface port and Twido comms port together (leave the setting as default).
Download the application serially to the Twido. Connect the TwidoPort to the PLC using the cable provided, then power cycle the PLC. The TwidoPort will derive it’s IP address from the PLC.
To assign an IP address, follow the steps below;
Select the ‘describe’ tab in TwidoSuite, then choose the appropriate PLC and Ethernet interface (this can be found in the hardware catalogue under ‘Network elements’, then ‘Modbus elements’).
Double click on the Ethernet Interface module and set the required IP address and gateway address (the mac address should be 255.255.255.0).
Double click on the serial port of the PLC and set it as Modbus (address 1 in this example). Link the Ethernet interface port and Twido comms port together (leave the setting as default).
Download the application serially to the Twido. Connect the TwidoPort to the PLC using the cable provided, then power cycle the PLC. The TwidoPort will derive it’s IP address from the PLC.
Note: The Twido range is discontinued and the possible replacement is the Modicon M221. The software to program this new controller is the EcoStruxure Machine Expert Basic also free. The software can automatically be migrated to this new platform but check with our support center your architecture to validate the migration. You can also use our product substitution tool to help you select the replacement for the twido: https://www.se.com/ww/en/product-substitution/ |
Released for:Schneider Electric UK
Explore more
Explore more