Search FAQs
Can I add additional contacts to an XD2G Joystick?
No, it is not permissible to add additional contact blocks to the XD2G Joystick controllers.
However, under the XD2G offer, we do manufacture units with two contacts per direction.
There are two other alternatives to add additional contacts:
However, under the XD2G offer, we do manufacture units with two contacts per direction.
There are two other alternatives to add additional contacts:
- Replace the XD2G with the XKDF Joystick range, this offer allows more contacts per movement.
- Use an additional relay such as a TeSys CAD32** or Zelio Relay RXZ***
Released for:Schneider Electric UK
Explore more
Range:
Explore more
Range: