Search FAQs
Why can't I find combination Motor Starters (e.g. GV2DM202) on the My Schneider site?
In the UK we do not offer pre-assembled combination starters, but the individual parts to make them up. The assembly is a very short and simple process.
Each starter is made up of a GV2 manual motor starter and a contactor (LC1D or LC1K) plus an adaptor to join the two together. The section of the catalogue for combination starters lists the part numbers of the individual parts required.
Example
D.O.L Revering starter GV2DM202**
This is made from the following:
Note
** refers to the coil voltage code eg BD for 24Vdc
Each starter is made up of a GV2 manual motor starter and a contactor (LC1D or LC1K) plus an adaptor to join the two together. The section of the catalogue for combination starters lists the part numbers of the individual parts required.
Example
D.O.L Revering starter GV2DM202**
This is made from the following:
- Motor Circuit Breaker GV2ME02
- Contactor LC2D09**
- Combination Block GV2AF3
Note
** refers to the coil voltage code eg BD for 24Vdc