{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the possibilities for replacing the DC coils of the LC1D range Tesys D contactors?

Article available in these languages: Korean

This depends on the current rating of the model you have:

Contactor rating 9 A to 65 A
A DC coil cannot be replaced. Typical contactor part numbers LC1D12BD (09-38A) and LC1D50ABD (40-65A)

Contactor rating 80 A to 150 A
The coil can be replaced on Tesys D contactors sold since 2001. Typical part number LC1D80BD.

Please refer to our latest catalogue for further information. You can find it here: digicat.se.com.

Please note that the coil on LC1D40-65** manufactured between 2001 and 2009 (non-everlink) could be replaced, but the replacement coils LXD-6** (along with their respective contactors) are all long obsolete.