Search FAQs
With the TSXCUSB485 cable, which Unitelway driver should I install for use in Windows Vista Business Edition 32?
The Unitelway V2.0 IE10 driver needed for the various Schneider programs which use the Unitelway protocol (PL7 Micro/Junior/Pro, Unity Pro , Control Expert, Vijeo Designer Lite) is available in the attachments.
It supports the following:
This attachment is an executable file which includes:
Note:
This executable is found in the V2.6 pack driver.
It supports the following:
- TSXCUSB485 USB cable
- TSXPCX1031 serial cable.
This attachment is an executable file which includes:
- The Unitelway driver
- The USB bus Windows driver
- The virtual serial port Windows driver
Note:
This executable is found in the V2.6 pack driver.
Released for:Schneider Electric UK
Attachment(s)
Explore more