{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the substitution of the GSKC product by the XPSAK module?

The equivalent of the GSKC safety module used for emergency stop monitoring in accordance with standard EN954-1 category 4 is the XPSAK module.

NB: For applications with contacts in series running over long wiring distances, you must check beforehand that the wiring resistance is less than the maximum value given in the instruction sheet for the XPSAK.


GSKC to XPSAK


PLEASE NOTE that XPSAK has also been replaced. Please refer to the attached XPSAK to XPSUAK converter tool for information on the new product.

Schneider Electric UK

Attachment(s)

XPSUAK_AK.pdfXPSUAK_AK.pdf [1.01 MB]
Explore more
Explore more
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.